Activating a license

Activate a license to enable the use of your system after a new install, an upgrade, or a migration. Activate licenses to enable features, such as software modules, or additional monitoring devices.

You can activate licenses online, directly from the Power Operation (PO) server if it has an Internet connection. You can also activate licenses offline, from an alternate internet-connected computer or smartphone. In both cases, you use the License Configuration Tool to activate licenses.

NOTE: You must have a valid Activation ID to activate a license.

To activate a license online:

  1. On the PO server, open the License Configuration Tool, and select Activate License. A message box is displayed.
  2. NOTE: You can access the License Configuration in the install location within ....\Schneider Electric\Power Operation\License Configuration Tool, or by clicking Start on the taskbar and choosing Schneider Electric > Power Operation License Configuration Tool.

  3. Read the information and select OK. The Activate License page opens.
  4. On the Activate License page, enter the Activation ID, and then select Activate.
  5. NOTE: By default, the activation method is set to Online.

    The license appears in the License Configuration Tool.

  6. Close the License Configuration Tool.

To activate a license offline:

  1. On the PO server, open the License Configuration Tool, and select Activate License. A message box is displayed.
  2. NOTE: You can access the License Configuration in the install location within ....\Schneider Electric\Power Operation\License Configuration Tool, or by clicking Start on the taskbar and choosing Schneider Electric > Power Operation License Configuration Tool.

  3. Read the information and select OK. The Activate License page opens.
  4. On the Activate License page, set Activation method to Offline.
  5. NOTE: By default, the activation method is set to Online.

  6. In the Initiate section, enter the Activation ID and select the location to save the activation request file. Click Download. The activation request file capabilityrequest.bin downloads to the selected location.
  7. Copy the capabilityrequest.bin file to a computer or a web-enabled device, such as a smartphone with Internet access.
  8. On the Internet-connected computer or device, open a Firefox or Chrome browser.
  9. NOTE: Internet Explorer is not supported.

  10. Browse to the Offline Licensing Web Portal (https://schneider-electric.flexnetoperations.com/flexnet/operationsportal/logon.do).
  11. Log in using the activation ID.
  12. Click the Devices drop-down and then select Offline Device Management. The Offline Device Management window opens.
  13. On the Offline Device Management page, select Choose File, and then select the capabilityrequest.bin file, and select Upload. The Download my License Response File window opens.
  14. In the Download my License Response File window, select Download to save the capabilityresponse.bin file.
  15. Copy the capabilityresponse.bin file to the PO server computer.
  16. TIP: If you are using a smartphone, try using a USB cable to copy the file.

  17. On the PO server, open the License Configuration Tool, and select Activate License. A message box is displayed.
  18. NOTE: You can access the License Configuration in the install location within ....\Schneider Electric\Power Operation\License Configuration Tool, or by clicking Start on the taskbar and choosing Schneider Electric > Power Operation License Configuration Tool.

  19. Read the information and select OK. The Activate License page opens.
  20. On the Activate License page, set the Activation method to Offline.
  21. NOTE: By default, the activation method is set to Online.

  22. In the Complete section, select the location of the capabilityresponse.bin file, and select Activate. The license appears in the License Configuration Tool.
  23. Close the License Configuration Tool.