Software prerequisites
The following software components are required for the operation of Power Operation. These software components will be installed during the Power Operation installation:
- NET Framework 4.8
- NET Core 8 (8.0.10) - Windows Desktop Runtime, ASP.NET Shared Frameworks, Runtimes, and Windows Server Hosting
- IIS URL Rewrite Module 2
- WebView2 Runtime
- Microsoft Visual C++ 2008 Redistributable
- Microsoft Visual C++ 2010 Redistributable
- Microsoft Visual C++ 2012 Redistributable
- Microsoft Visual C++ 2015-2022 Redistributable
- Visual FoxPro OLE DB Provider