Upgrading Project TGML Graphics
To upgrade TGML graphics to include the latest changes made to the graphics components from previous versions, do the following:
- Open Power Operation Studio.
- Navigate to Projects > Migration Tool > Power Operation Migration Tool.
- In the Power Operation Migration Tool, select the project you want to upgrade, and select the Update Reference Component Definitions checkbox.
- Click Migrate.
- Open Graphics Editor.
- Navigate to the Connection Debugger and select Create Configuration File.
The OneLineConfiguration.json file is updated to include the Advanced One-Line logic needed to support the latest updates for standard components.