Windows Updates

warning

potential compromise of System availability, integrity, and confidentiality

Apply the latest updates and hotfixes to your Operating System and software.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

Be sure that all Windows updates and hotfixes—especially Windows security updates—are regularly applied to machines running Power Operation and Power Monitoring Expert.

If compatibility issues arise from Windows updates, they are considered high priority by the Power Operation with Advanced Reporting and Dashboards development team. They are evaluated and resolved to deliver patches to enable the continued use of Windows security updates.