Configure

This section describes the different tools and tasks for configuring Power Operation.

Use the links in the following table to find the content you are looking for:

Section Description
Configuration prerequisites Things to consider to help you prepare for configuring a Power Operation project.
Changing configuration on a running system Describes configuration changes that can be made on a running system.
Configuration tools An introduction to the Power Operation configuration tools.
SCADA Projects Creating a Power Operation project using Project Setup, and compiling, backing up, an restoring a project.
Devices

Information and tasks on how to configure and work with:

  • Device profiles
  • Device types
  • Device tags
  • Profile Editor projects
  • Profile Studio projects
  • Adding I/O devices to the project
  • Alarms
Power Operation Runtime

How to configure and work with:

  • Graphics pages
  • Animated one-lines
  • Menus and pages
  • Basic reports
  • LiveView
  • Notifications
Web Applications

How to configure and work with:

  • Alarms
  • Diagrams
  • Web Applications settings
Applications Information on extending the capabilities of Power Operation by configuring applications.
Managing user accounts, roles, and mapping Configure and manage user access.
Customize default behaviors How to use Cicode to customize a project, localizing a project, and running PO as a Windows Service.
System Startup and Validation Checks How to validate your configured system on startup.
Distributed systems

How to configure:

  • Advanced Reporting and Dashboards Module
  • Power SCADA Anywhere
  • EcoStruxure Web Services
  • Time synchronization and time zone settings
  • OFS time stamping
  • OPC-DA Server and Client
Redundant systems How to configure a redundant server.

For more detailed resources on configuration, see the Configure references section.