Adding a serial device

NOTE: These instructions assume that you have two I/O Servers, and that you will be renaming ports.

To add a serial device to a project:

  1. From the Power Operation Studio screen, display the project to which you want to add the device.
  2. Click Topology > I/O Devices > I/O Device Manager.

    The I/O Device Manager welcome screen displays.

  3. Click Create an I/O Device in the project, then click Next.
  4. At the Choose profile screen, select the first device profile that you want to use to add a device to the project. Click Next.
  5. At the Enter instance information screen, type a descriptive profile name, for example: CM4Bay1Circuit1 (no spaces or punctuation; to allow space in Power Operation, the preferred limit is 16 characters). The Comment field is stored in the equipment.dbf file. Click Next.
  6. At the Select I/O servers screen, choose the primary and standby servers. You can add information for the standby server if you click Supports Redundancy. Click Next.
  7. If you choose to add an optional sub-profile: At the Configure Sub-Profile Communications Method screen, choose the communications method used for the first sub-profile in this project. Click Next.
  8. At the Communications Settings screen, enter the information for each server (com port, baud rate, etc.). If you click Same as Primary for standby, you will use the same addresses for the primary and standby. Click Next.
  9. At the Port Settings screen, you can rename each of the ports.
  10. When you finish adding the last sub-profile, the Ready to perform action screen displays. Click Next.

    After the devices are added, a screen displays telling you that the project was updated successfully.

    • To view a detailed list of all the devices and all operations performed in the project, click View audit log. The list displays after the device is added.
    • To continue adding or removing devices, click Next. Repeat steps 3 through 10.

  11. When you finish adding devices, click Finish at the Project updated successfully screen.

    If you clicked View audit, the list displays.

    If you did not click Add/remove, the I/O Device Manager closes.

  12. Compile the project. Correct any compile errors and then compile the project again.
  13. Click Run to view the runtime environment.