Create Real-Time Data Views

Create and view LiveView templates and views for real-time data tables. Some basic predefined templates are included with the software; you can create new templates or make copies of the predefined templates and edit the copies.

Before you view LiveView templates and views, you must set up data acquisition parameters. To do this, use the Application Configuration Utility. See Set up data acquisition parameters for instructions.

NOTES:

  • If you find that a predefined table does not include enough cells for the data you want to display, use the duplicate feature to make a copy of the predefined table. Then add the needed cells to the duplicate.
  • If you install Matrikon Explorer on the same computer as Power Operation 2024, the LiveView and reporting features will not launch. To prevent this, install Matrikon before you install Power Operation 2024. If you install Matrikon after you install Power Operation, you need fix the issue in this way: Go to IIS > ISAPI Filters, and then reset the DLL that is already selected (click browse and re-select v4.0.30319 aspnet_filter.dll). Click OK.)

You can only view data in these templates if your system is online and you are connected to devices that provide data.

To set up LiveView real-time data tables in the Power Operation Runtime:

  1. Open the LiveView Viewer in your Internet browser:
  2. http://localhost/LiveViewViewer

  3. Create a custom template or choose an existing template.
  4. Select devices from which to show real-time data
  5. Save the view, providing a name.
  6. Keep track of the names of your saved views. You will need to use them when you create menu items that display these views in the Power Operation Runtime.