Enable Waveforms

On the Create Device Profiles tab, in the Onboard Alarm Tags sub-tab, there is a Waveform check box. Check the box for each alarm tag for which you want to be able to view waveforms. On the device, the alarm must also be set up for the waveform to be captured on event and stored in one of the device’s data logs.

To acquire waveforms for Sepam, use the CET manual. For PowerLogic devices, refer to the PMCU help file.

As device information is polled and received by Power Operation, the waveform becomes available for viewing. See The Alarm Log in Viewing Alarms and Events for information on viewing waveforms in the Power Operation Runtime.