Design

Easergy CL110 and TH110 sensors are installed in the substation. The sensors wirelessly send measurement data to the ZBRN32 access points. The access points are connected to SMDs through Modbus serial communications. The SMDs are connected to Power Operation through an Ethernet connection.

Power Operation has a pre-configured device profile for the SMD. See Configuring a thermal monitoring device profile for more information.

NOTE: If you are using Power Operation 2024 with Advanced Reporting and Dashboards and want to set up reports and dashboards to display substation data, refer to the Thermal Monitoring of Medium Voltage (MV) Substations section in the PME System Guide on www.se.com or the Schneider Electric Community.