Export and import One-Time Password settings
You can copy and use one-time password settings on multiple server computers.
NOTE: When you import password settings into another server, you will overwrite any password settings that already exist there. You are not simply adding the new password settings to the existing ones.
To copy and use one-time password settings on multiple server computers:
- In the Application Configuration Utility: select the Security drop down and then select One-time Password.
- Select Export. A file named
ExportedOTPConfiguration.xmlis generated. You can rename it if you wish. Save it where you can access it from other servers, or copy it to a portable drive. - From a server to which you want to import the password settings, select Import. You are prompted for a location.
- Browse to the location where you placed the XML file. Select Open and accept the XML file.