Opening Notifications Settings
Open Notifications Settings from the Power Operation Runtime.
NOTE: Notifications Settings can be customized to open anywhere in the Power Operation Runtime.
In the Power Operation runtime, select Alarm Log > Notifications Settings.
Notifications Settings appears:
Assuming notifications from Event Notification Module (ENM) were not migrated, when you first open Notifications Settings, a notification is included by default. This default notification includes an alarm filter that includes all alarms in the system, a fictitious recipient, a message template, and a schedule.
Create your system notifications either by editing and duplicating the default notification, or adding a new one.