Devices
Use Profile Studio to configure Power Operation in accordance with IEC 61850-standard engineering workflows.
Use Profile Editor to create device types and device profiles outside of the IEC 61850-standard engineering workflow.
Use Profile Studio to configure Power Operation in accordance with IEC 61850-standard engineering workflows.
Use Profile Editor to create device types and device profiles outside of the IEC 61850-standard engineering workflow.
Last updated: January 21, 2026
© 2026 Schneider Electric. All Rights Reserved. Home Safety precautions