Compile the project
In Power Operation Studio, click Compile
. If you are promoted to save your changes, click Save.
If there are errors or warnings after the project is compiled:
- At each error, click GoTo, which opens the location where the error occurred.
- Using the information in the error message, correct the error.
- After all errors are addressed, re-compile to verify that the errors are removed.
For additional information, click Help at the error screen.