Deploying a Power Operation project

Distribute projects and related updates to multiple clients in your Plant SCADA system by using a deployment server. In the Plant SCADA help file ( ..\Program Files (x86)\Schneider Electric\Power Operation\v2024\bin\Help\SCADA Help), see the Deployment section for information on preparing, configuring, using, and troubleshooting deployment servers and clients. For more information, visit the AVEVA Plant SCADA Forum.

Advanced one-line files will not be automatically included in a deployment.

To include advanced one-line files in deployment:

  1. In Power Operation Studio, in the Setup activity, in the File Name column, enter the following file names in two respective rows:
    • AdvOneLine.ini.txt
    • AdvOneLine.csv

  2. Select Save.
  3. Select Compile the active project.
  4. NOTE: If the one-line settings are modified in any way after being added to the Setup activity, you must recompile the project in order to include the changes in the deployment.

  5. Deploy the project. For more information, see the Plant SCADA help file.