Power Operation Runtime
                                                 warning
warning
unintended equipment operation
| ● | Do not use the software or devices for critical control or protection applications where human or equipment safety relies on the operation of the control action. | 
| ● | Do not use the software to control time-critical functions. | 
| ● | Do not use the software to control remote equipment without proper access control and status feedback. | 
Failure to follow these instructions can result in death or serious injury.
Extensively test the deployed project to ensure that permissions are applied as intended because Power Operation lets you set user permissions on runtime graphical objects.
The Power Operation Runtime is where the end user views system information that is added in the design-time pages. The Power Operation Runtime can include:
- One-line diagram pages with interactive objects
- Alarm and event pages
- Analysis pages (trends and waveforms)
- Basic reports
If Power Operation includes Advanced Reporting and Dashboards Module, you can configure the Power Operation Runtime to includes dashboards and advanced reports.