Restore the Power Operation Studio project
To restore the project:
- In Power Operation Studio, select Projects
. - Select the Backup drop down and then select Restore.
- Beside the Backup file text field, select Browse, and then browse to the location of the project file you will use to restore.
- (Optional) Select Select all included projects.
- In the To area, select Current Project.
- In the Options area:
- Select Configuration files to restore backed up INI files and the TimeSyncConfig.xml file (used to store time synchronization settings).
- Select Select sub-directories. The sub-directories included in the earlier backup will be listed.
- Select OK.