Tag Debugger
The Tag Debugger is a TGML graphic component that lets you diagnose and troubleshoot devices from the Power Operation Web Applications. You can use it to check device status, read values from, and write values into the registers of configured devices.
warning
unintended equipment operation
● | Do not use the software or devices for critical control or protection applications where human or equipment safety relies on the operation of the control action. |
● | Do not use the software to control time-critical functions. |
● | Do not use the software to control remote equipment without proper access control and status feedback. |
Failure to follow these instructions can result in death or serious injury, or equipment damage.
Before you use the Tag Debugger, add the component to a diagram, and then configure it. The topics in this section outline how to configure and use the Tag Debugger, and includes the following topics: