Exporting alarm menus

To export an alarm menu:

  1. Log in to PO Web Applications (https://localhost/webhmi or https://ipaddress/webhmi).
  2. Select ALARMS:


    The following screen is displayed:


  3. On the Home view, select the 3 dots, and then select Export:


  4. Select the JSON file export location, and then select Save.

  5. Check the file in the folder to confirm that the Alarm Menus were exported.

For reference information, see:

For information on how to use Alarms, see Alarms.