Managing CAE user roles

You can define permissions for system components. Model permissions for roles are deactivated by default for newly added roles.

Recommendations:

  • Assign roles only the essential privileges needed to perform their job.

  • Follow user account management tasks as described by your organization or contact your network administrator.

  1. Open Cybersecurity Admin Expert.
  2. Select ROLES tab:
    • Add a new role: click the Add role button, edit details.
    • Edit role: select role and edit details.
    • Delete role: select a role and click the Trash icon. The SECADM role can not be deleted.
  3. Click Save changes.

You can disable the ability to connect to a device through its front panel using the security administrator (SecurityAdmin) user account. This is available in the in the SECURITY SETTINGS tab for Substation and Feeder Automation architectures.