Best practices for creating and editing components and/or TGMLs
When creating components and/or TGMLs, consider implementing the following best practices:
- Avoid combining reference and non-reference instances in the TGML or TGML component document. This can cause complexities in the component hierarchy.
- Use reference components when creating custom components, as you can use the Reference Definition Updater to update the component and all its instances in TGML and components at the same time. This Reference Definition Updater will not update non-reference components.
- Avoid creating cyclic component dependencies, which can make system behavior difficult to predict and maintain.
When editing or working with components and/or TGMLs, consider implementing the following best practices:
- When working with components, avoid making changes at the component definition level directly in the Object Browser. If customization is required, it is best to duplicate the component and make changes to the duplicate.
- When editing a TGML component, ensure that only one TGML component file is open.
- When editing a TGML component, ensure that any other TGML component files are saved.
- Avoid deleting or editing any properties from components' Definitions (TGML > Definitions > Component). If a component property, such as ID, is mistakenly removed, you can recover it by re-entering the property again using the same syntax as was used before the removal.