Adding a Linear Gradient

You add a linear gradient to give an object a smooth, varying hue from one point to another.

For more information, see section the Gradients Overview section.

To add a linear gradient:

  1. In Graphics Editor, in the work area, select the object on which to apply the gradient.
  2. On the Options toolbar, click Fill to open the Color/Gradient palette.
  3. Click the Gradient tab.
  4. Click the box with the gradient you want to use.

In the Objects pane, a LinearGradient element and two or more GradientStop elements are added to the object.