Adding a Radial Gradient
You add a radial gradient to give an object a smooth, varying hue from a center point to the periphery.
For more information, see the Gradients Overview section.
To add a radial gradient:
- In Graphics Editor, in the work area, select the object to which you want to add the radial gradient.
- On the Options toolbar, click Fill to open the Color/Gradient palette.
- Click the Gradient tab.
- Click the radial gradient you want to use.
In the Objects pane, a RadialGradient element with two or more GradientStops are added to the object.