Adjusting a Radial Gradient
When you use the Fill – Gradient palette, you may need to adjust the color or some other aspect of the appearance.
Adjusting a radial gradient involves first finding the specific object in the Objects pane and then changing the gradient parameters of the RadialGradient or the GradientStop elements.
You can adjust a radial gradient to suit current requirements. For more information, see the Gradients Overview section.
To adjust a radial gradient:
- In Grahics Editor, in the work area, select the object with the radial gradient that has to be adjusted.
- In the Objects pane, locate the object.
- Expand the object elements to display the RadialGradient element with its GradientStops.
- Select the RadialGradient element.
- To change the gradient target (the area or the stroke), in the Target area, in the Attribute box, switch between Fill and Stroke.
- To change the gradient focus (the beginning of the radial gradient), in the Position area, in the Focus box, type x and y-coordinates between (0,0) and (1,1). To change how far the gradient will reach (a kind of gradient end point periphery), a circle or ellipse is used.
- In the Position area, click the periphery ellipse Center, and type x and y- coordinates between (0,0) and (1,1).
- In the Position area, complete the circle/ellipse by selecting RadiusX or RadiusY, and type values between 0 and 1 to define the reach of the periphery.
- To change any of the gradient colors (the “start” and “stop” colors), in the Appearance area, in the Color box, click a color in the Color palette, or type the a hexadecimal color code.
- To change the offset (where the “start” and “stop” colors will be positioned, relative to the RadialGradient focal point), in the Position area, in the Offset box, type a value between 0 and 1.