Arranging Objects

If an object more or less overlaps another object, you may want to arrange them. You can move an object so that it appears behind or in front of other objects.

You can also move a graphic object to the very back or the very front of the stack.

You can arrange one or more selected objects in four different ways:

  • Bring to Front: Bring the object(s) to the top position
  • Bring Forward: Bring the object(s) one position up
  • Bring Backward: Bring the object(s) one position down
  • Bring to Back: Bring the object(s) to the bottom position

NOTE: When you select more than one object, the selected objects keep their internal order during the arrangement procedure.

NOTE: The Arrange menu options list shows how the objects can be arranged.

You arrange objects that more or less overlap each other to put certain objects in front of or behind other objects.

To arrange objects:

  1. In Graphics Editor, in the work area, select the object that you want to move backward or forward.
  2. On the Options toolbar, click Arrange , and then click the required option.