Editing a Text Path

You edit a text path to change its appearance or other properties. The text path is in fact a curve and can be modified like any other curve, but you can no longer edit the text itself.

For more information, see the Adding Text and Textboxes section.

To edit a text path:

    In Graphics Editor, in the work area, select the text path.

  1. In the Properties pane, edit the properties (Fill, Opacity, Stroke, StrokeDashArray, StrokeWidth, or Visibility).
  2. Double-click the path and drag the vertices to change the shape of the path.
  3. Click outside the textpath to clear the selection.