Flipping Objects
Flipping an object means that you replace the object with a reflection of the original object on a horizontal or vertical axis.
You flip one or more objects to reflect them in a horizontal or vertical direction.
To flip an object:
- In Graphics Editor, in the work area, select the object you want to flip.
- On the Options toolbar, click the Flip button
to open the flip axis menu.
- Click the Horizontal button
to reflect in a horizontal direction and the Vertical button
to reflect in a vertical direction.