Drawing a Circle
In Graphics Editor, use the Ellipse tool to draw a circle, that is, a line forming a closed loop, every point on which is a fixed distance from a center point. A circle is actually a special case of an ellipse. In an ellipse, if you make the major and minor axis the same length, the result is a circle, with both foci at the center.
You draw a circle when you need a figure forming a closed loop where every point is a fixed distance from the center point.
To draw a circle:
- In Graphics Editor, in the Layers pane, select the layer where you want to draw the circle.
- On the Drawing toolbar, click Ellipse.
- In the work area, click Shift while dragging the pointer from where you want the circle to begin to where you want it to end.
- On the Drawing toolbar, click Select.
- In the Properties pane, in the Name box, type the name of the circle.
NOTE: You only need to name the drawing object if you will be binding the object. Naming the object now will help you identify the object later.
- On the Options toolbar or in the Properties pane, adjust the appearance of the circle.
- On the File menu, click Save.