Drawing a Line
Use the Graphics Editor Line tool to draw a straight line, that is, a line between two points.
You can set stroke, style and width properties to change the line color, pattern and thickness.
You draw a line when you want to draw an extending one-dimensional figure that has no curvature.
To draw a line:
- In Graphics Editor, in the Layers pane, select the layer where you want to draw the line.
- On the Drawing toolbar, click Line.
- In the work area, click where you want the line to start and drag to where you want it to end.
- On the Drawing toolbar, click Select.
- In the Properties pane, in the Name box, type the name of the line.
- On the Options toolbar, or in the Properties pane, adjust the appearance of the line.
- On the File menu, click Save.
NOTE: You only need to name the drawing object if you will be binding the object. Naming the object now will help you identify the object later.