Drawing a Square

You draw a square when you need a figure with four equal sides and four 90° angles.

To draw a square:

  1. In Graphics Editor, in the Layers pane, select the layer you want to draw the square.
  2. On the Drawing toolbar, click Rectangle.
  3. In the work area, press Shift and click where you want the square to begin and drag to where you want it to end.
  4. On the Drawing toolbar, click Select.
  5. In the Properties pane, in the Name box, type the name of the square.

    NOTE: You only need to name the drawing object if you will be binding the object. Naming the object now will help you identify the object later.

  6. On the Options toolbar or in the Properties pane, adjust the appearance of the rectangle.
  7. On the File menu, click Save.