Panel Navigation
When you use graphics in a panel, you can configure which target location is to be opened when you perform an action (e.g. a mouse click) on a target object linked to the graphic. You can configure the graphic in Graphics Editor by adding an invoke function script. In Diagrams, you link the graphic to the target object you want to open when you perform the action.
A target object can be opened from a graphic in any of the following target locations:
- Floating window
- New window
- Parent
- Self
- Target
- Top
- Work area
You can also use the invoke function script to give the user the ability to navigate back and forward to a previously visited view.