TGML Limitations
In some implementations, for example, Microsoft GDI+, there are limitations to TGML attributes.
Positional and Size-Related Limitations
Positional attributes have a limitation of +/- 10.000 pixels. Size-related attributes have a limitation of 10.000 by 10.000 pixels. That is, no TGML figure can have a size that exceeds 10.000 by 10.000 pixels. This size limitation also applies for the canvas. The following TGML attributes are affected by the limitations:
- Top
- Left
- Height
- Width
- Length
- X1
- X2
- Y1
- Y2
- Points
- RadiusX
- RadiusY
- StartPoint
- EndPoint
- ContentHeight
- ContentWidth
- FontSize
- StrokeWidth