TGML Ellipse

The <Ellipse> element defines an ellipse.

Attribute Type Description

Fill

Brush

Specifies how the interior of the shape is painted.
Default: "None"
Inheritable: Yes
Animatable: Yes

Height

Double

The height of the ellipse.
Inheritable: No
Animatable: Yes

Left

Double

The x coordinate of the upper left corner of the ellipse.
Default: "0"
Inheritable: No
Animatable: Yes

Opacity

Double

A value between "0.0" (transparent) and "1.0" (opaque)
Default: "1.0"
Inheritable: No
Animatable: Yes

Stroke

Brush

Describes how the line is painted.
Default: "#000000"
Inheritable: Yes
Animatable: Yes

StrokeDashArray

Array of Double

The pattern of dashes and gaps used to outline shapes:
"<dash> [ <gap> <dash> <gap>...]"
If the array only specifies the first dash, the line is patterned as if a gap with the same length as the dash was specified.
An array with only one dash set to "0" will result in a line without any pattern.
Default: "0"
Inheritable: Yes
Animatable: Yes

StrokeWidth

Double

The width of the outline of a line.
Default: "1"
Inheritable: Yes
Animatable: Yes

Top

Double

The y coordinate of the upper left corner of the ellipse.
Default: "0"
Inheritable: No
Animatable: Yes

Visibility Visibility

Specifies if the element is visible or not.
Default: "Visible"
Inheritable: No
Animatable: Yes

Width

Double

The width of the ellipse.
Inheritable: No
Animatable: Yes

Example:

Copy
<TGML>

    <Ellipse Left="10" Top="10" Width="100" Height="50" Fill="#FFFF00" Stroke="#000000"/>

    <Ellipse Left="120" Top="10" Width="50" Height="50" Fill="#FFFF00" Stroke="#000000"/>

</TGML>

Example on screen: