TGML SignalChange Event Methods
The following table contains an overview of the methods that are specific for the SignalChange event object:
Method | Description |
---|---|
getStatus() |
Returns the status of the signal: |
getPresentationValue() |
Returns the value of the bound signal as a "presentation value". For more information, see section 33.12 “TGML Signal Binding: <Bind>” on page XXX. |
getUnit() |
Returns the unit of the bound signal as a string. |
getValue() |
Returns the value of the bound signal. |