Enable and Disable Alarms
Disable and Enable alarms from the All Alarms, Active Alarms, or Unacknowledged Alarms pages.
To disable alarms:
-
In WebHMI, click on the ALARMS tab.
-
In the View Library, click All Alarms, Active Alarms, or Unacknowledged Alarms.
-
Right-click an alarm > Open Details.
-
Click the Disable button.
-
Click the Submit button.
To disable multiple alarms:
Do one of the following:
-
You can disable more than one alarm at a time by selecting multiple rows, right-clicking > Disable Selected. Or choose Options menu > Disable Selected.
-
You can disable all alarms by choosing Options menu > Disable All.
To view disabled alarms:
-
In the View Library, click Disabled Alarms.
To enable alarms:
-
In WebHMI, click on the ALARMS tab.
-
In the View Library, click Disabled Alarms, Active Alarms, or Unacknowledged Alarms.
-
Right-click an alarm > Open Details.
-
Click the Enable button.
-
Click the Submit button.
-
Click the Close button.
-
In the View Library, click All Alarms.
To enable multiple alarms:
Do one of the following:
-
You can enable more than one alarm at a time by selecting multiple rows, right-clicking > Enable Selected. Or choose Options menu > Enable Selected.
-
You can enable all alarms by choosing Options menu > Enable All.
NOTE: Disabling and re-enabling an active alarm with the default Plant SCADA INI parameter will result in two active instances of the alarm in Alarm History.