Web Applications settings

TIP: You can open the Settings page from the SETTINGS link in the Web Applications banner.

Use the Settings page to access Web Applications settings and configuration tools.

NOTE: Access to this application or function is controlled by user privileges. See Managing user accounts, role names, and mapping for details.

TIP: Use Search, in the Settings Library, to find the settings and tools you are looking for based on keywords.

The Settings page consists of a Settings Library and a configuration area. The Settings Library provides access to the following settings and tools:

Category Settings/Tools
Alarms Alarm Views
Integrations Authorized Hosts
Personalization Personal Preferences
System localization
System Theme
Security Session timeout
Web Redundancy Web redundancy