Enable and Disable Alarms
Disable and Enable alarms from the All Alarms, Active Alarms, or Unacknowledged Alarms pages.
To disable alarms:
- In WebHMI, select on the ALARMS tab.
- In the View Library, select All Alarms, Active Alarms, or Unacknowledged Alarms.
- Right-click an alarm > Open Details.
- Select the Disable button.
- Select the Submit button.
To disable multiple alarms:
Do one of the following:
- You can disable more than one alarm at a time by selecting multiple rows, right-clicking > Disable Selected. Or choose Options menu > Disable Selected.
- You can disable all alarms by choosing Options menu > Disable All.
To view disabled alarms:
- In the View Library, select Disabled Alarms.
To enable alarms:
- In WebHMI, select on the ALARMS tab.
- In the View Library, select Disabled Alarms, Active Alarms, or Unacknowledged Alarms.
- Right-click an alarm > Open Details.
- Select the Enable button.
- Select the Submit button.
- Select the Close button.
- In the View Library, select All Alarms.
To enable multiple alarms:
Do one of the following:
- You can enable more than one alarm at a time by selecting multiple rows, right-clicking > Enable Selected. Or choose Options menu > Enable Selected.
- You can enable all alarms by choosing Options menu > Enable All.
NOTE: Disabling and re-enabling an active alarm with the default Plant SCADA INI parameter will result in two active instances of the alarm in Alarm History.