Shelve and Unshelve Alarms
Shelve and unshelve alarms for minutes, hours, or days, from the All Alarms, Active Alarms, or Unacknowledged Alarms pages.
To shelve alarms:
Alarms will be shelved until the assigned duration has elapsed.
- In WebHMI, select on the ALARMS tab.
- In the View Library, select All Alarms, Active Alarms, or Unacknowledged Alarms.
- Double-click an alarm.
- Select the Shelve button.
- In the Shelve Alarm pop-up window, configure the shelve duration and select the Submit button.
- In the View Library, select Shelved Alarms to view the shelved alarms.
To shelve multiple alarms:
Do one of the following:
- You can shelve more than one alarm at a time by selecting multiple rows, right-clicking > Shelve Selected. Or choose Options menu > Shelve Selected.
- You can shelve all alarms by choosing Options menu > Shelve All.
To unshelve alarms:
Unshelve alarms prior to their shelved duration elapsing.
- In the View Library, select Shelved Alarms, Active Alarms, or Unacknowledged Alarms.
- Double-click an alarm.
- In the Alarm Definition pop-up window, select the Unshelve button.
- Select the Close button.
To unshelve multiple alarms:
Do one of the following:
- You can unshelve more than one alarm at a time by selecting multiple rows, right-clicking > Unshelve Selected. Or choose Options menu > Unshelve Selected.
- You can unshelve all alarms by choosing Options menu > Unshelve All.