Viewing waveforms
View waveforms to investigate power quality events and identify root causes of disturbances. You must have an associated alarm with a corresponding timestamp present in the WebHMI to view a waveform within the WebHMI.
To view waveforms:
- In the alarm viewer, open an existing Incident history view or alarm history view from the View Library or add a new View.
- Find the incident or alarm for which you want to view waveforms, and select Details
. You can also open Details by double-clicking the incident or alarm instance. - In Details, select Waveforms.
TIP: Select Open Representative Waveform to see the representative waveform for this Incident or alarm instance.
- View the waveforms associated with the incident or alarm instance.
(Optional) Select Inspect a waveform to see more details and to analyze the waveform.
For information on how to configure Alarms , see Alarms configuration.
For information on interpreting waveforms, see Waveform Analytics.
For information on setting up the Waveform Extractor, see Configuring the Waveform Extractor.