Basic Reports
You can create, view, save, and print basic reports
Prerequisites
Before you can create and view basic reports, the following requirements must be met:
- You must set up reporting in the Power Operation Runtime. See Set up the Power Operation Runtime for basic reports.
- There must be data logged for the project. See Analysis Page for help.
NOTE: If the Schneider Electric CoreServiceHost has not been refreshed after devices or topics have been added, you should clear the cache and refresh the platform in order to access the new devices or topics. See Clear cache and refresh platform for instructions.
After you have logged trend information, you can create and view basic reports. In Power Operation Runtime, select the Reports tab and then choose the basic report type you want to create: