Configuring the Setpoint Display Bar to monitor electrical health

Use the Setpoint Display Bar to measure and display a single parameter.

To configure the Setpoint Display Bar:

  1. In Graphics Editor, from the Components pane > Power Measurement category, drag the Setpoint Display Bar to the work area.
  2. In the Objects pane, bind your equipment to the Setpoint Display Bar.
  3. In the Properties pane, set the following to match the equipment's operational ranges:
    • The minimum and maximum values.
    • Appropriate values for each setpoint.
    • Associated colors.
  4. In the Properties pane, in the Name property, enter a name using the following format: EquipmentName.Item Name.