Create a New Project
To create and configure a new Power Operation project, see SCADA Projects.
The new project will have a default cluster, computer, network, and servers (Alarm, Trend, Report, and I/O). The project will also include two defined I/O devices, zOL (used for Advanced One-line) and NetworkTagsDev (used for communication purposes). Furthermore, the PLS_Include project is included with the main project. The PLS_Include contains the standard Power Operation cicode, labels, fonts, alarm categories, parameters, graphics, and tools.