Alarms references
This section contains reference information related to using Alarms.
Use the links in the following table to find the content you are looking for:
Topic | Content |
---|---|
Alarms UI | Contains detailed information on the Alarms UI. |
Waveforms UI | Contains detailed information on the Waveforms UI. |
Timeline Analysis UI | Contains detailed information on the Timeline Analysis UI. |
Alarm to Incident Mapping | Details the mapping of alarm types to Incidents. |
Alarms terminology | A list of commonly used terms related to Alarms in Power Operation. |