Graphics Editor references
The topics in this section contain supplementary information about Graphics Editor.
Use the following links to find the content you are looking for:
| Topic | Content | 
|---|---|
| Saving a Graphic | Information on saving a graphic. | 
| Printing Graphics | Information on printing graphics. | 
| Graphics Editor Libraries | Information on accessing Graphics Editor's libraries of brushes, components, and snippets. | 
| Graphics Editor Keyboard Shortcuts | Keyboard shortcuts you can use with Graphics Editor. | 
| Graphics Editor Console | Information on the Graphics Editor Console. | 
| Graphic Object Position | Information on how to check the position and size of a graphic object using the graphic object position bar. | 
| Drawing with Graphics Editor | Topics on Graphics Editor drawing tools, which you can use to add lines, polylines, curves, polygons, rectangles, ellipses, arcs, pies, texts, and textboxes to a graphic. | 
| Graphics Editing Tools Overview | Topics on using Graphics editing tools. | 
| Documenting and Saving a Component | Information on how to document and savea component. | 
| Graphics Editor | Contains detailed information on the Graphics Editor UI. | 
| Workflows | Topics on Graphic Editor workflows. |