Motor

A motor is an electrical device, which converts electrical energy into mechanical energy, using the principles of electricity and magnetism.

The different types of motors that are supported in the Power Operation are:

  • ANSI motor
  • IEC motor
  • AC motor
  • DC motor

The bind properties available for ANSI/IEC motors are:

  • DestBusColor
  • IsMotorOn
  • SourceBusColor

AC/DC motors has only one bind property; BusColor.

The graphic representation of the default position and the bind property is explained in the below table:

Type Bind Property Description Graphic
All NA Motor is in default position. A simplified electrical circuit diagram displays a single wire connected to a motor, represented by the letter "M" inside a circle. An arc-shaped symbol is positioned over the wire, indicating a switch that can either connect or interrupt the circuit path. The diagram appears to illustrate a basic control concept involving a motor and a switch.
ANSI/IEC motors IsMotorOn Motor is On.
If the motor is Off, the circuit representation looks as shown.
AC/DC motors BusColor Sets the bus color.