Switch

A switch in an electronic device, which is used to interrupt the flow of electricity or electric current.

The different types of switches that are supported in the Power Operation are:

Type Description
ANSI type ANSI SW_General
SW_Isolated
IEC type SW_Fused
SW_Fused_Isolated
SW_General
SW_Knife

The bind properties available for switches are:

  • TopBusColor
  • IsSwitchOn
  • BottomBusColor

The graphic representation of the default position and the bind properties is explained in the below table:

Bind Property Description Graphic
NA Switch is in default position. Diagram features a vertical line intersected near the top by a circle. Below the circle, a diamond shape intersects the same vertical line at an angle. The visual layout is a symbolic representation of a switch in default position.
IsSwitchOn Switch is On.
If the switch is Off, the circuit representation looks as shown.