Transformer

A transformer is a device that transfers electrical energy from one electrical circuit to another without any change of frequency through the process of electromagnetic induction.

The different types of transformers that are supported in the Power Operation are:

  • Trans_nd_1
  • Trans_nd_2
  • Trans_sd_1
  • Trans_sd_2
  • Trans_ss_1
  • Trans_ss_2

The bind properties available for transformer are:

  • TopBusColor
  • BottomBusColor

The graphic representation of the default position and the bind properties is shown in the below table:

Bind Property Description Graphic
NA Transformer is in default position. Diagram displays a vertical line intersecting two circles that are aligned one above the other. The circles slightly overlap at their edges, and the vertical line passes through the center of both, extending beyond the top and bottom of the arrangement. The layout represents a transformer in default position.
TopBusColor Sets the bus color.
BottomBusColor
  • TopBusColor
  • IsTripped
  • IsClosed
  • RkdPos
  • BottomBusColor
  • EarthSwitchClosed