Utilities

Utility is a commercial entity that owns and operates equipment and facilities for the generation, transmission, and distribution of electric energy.

The different types of utilities that are supported in the Power Operation are:

  • Util_nd_1
  • Util_nd_2

Utility has only one bind property; BusColor.

The graphic representation of the default position and the bind property is shown in the below table:

Bind Property Description Graphic
NA Utility is in default position. A minimal black and white diagram features a large, bold letter "U" centered inside a circle. The circle is outlined with a thin black line. A short vertical line extends downward from the bottom of the circle, forming a shape similar to a lollipop. The layout represents a utility in default position.
BusColor Sets the bus color. A minimal red and white diagram features a large, bold letter "U" centered inside a circle. The circle is outlined with a thin line. A short vertical line extends downward from the bottom of the circle, forming a shape similar to a lollipop. The layout represents a utility in default position.