Before you add a project
Before you start adding data in the project, make sure that you have:
- Used the Profile Editor to add all of the device types, device profiles, and projects.
- Created a project; from the Power Operation Studio, added clusters, network addresses, and servers.
- Exported devices from the Profile Editor.
- Added devices into the Power Operation project, using the I/O Device Manager.