Edit generic tag addresses

This window displays when you select Edit for an address of a non-PowerLogic compatible device type, such IEC 61850 or DNP3.

The variable tag properties used in this screen are described in a topic in the Plant SCADA help file. For detailed information, see Add a Variable Tag in the Plant SCADA 2023 help file: ..\Program Files (x86)\Schneider Electric\Power Operation\v2024\bin\Help\SCADA Help