Finish

Use Finish to compile and run the project.

Select Compile and Run Project to view the project in the Power Operation Runtime. In runtime, verify correct device communication using the Tag Viewer screen or by viewing any Communication Failure Alarms.

You can also use Finish to open the following Power Operation project development tools to further customize your project:

  • Open Power Operation Studio to make a variety of changes to the project.

    Many of the settings made by Project Setup are included in the Parameters file: Power Operation Studio > Settings > Parameters. You can also change these parameters in that file.

    NOTE: If you cannot make the newly-added project active, close, and then re-open Power Operation Studio.

  • Open Graphics Builder to create and edit the project graphics pages.
  • Open Application Config Utility to edit or set up many project features.

When you are finished, select Finish to close Project Setup.